This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我上午参考您给的链接尝试实现读取数据的功能,但是无法使用timer1GetValue()函数,而且报错挺多的,麻烦您帮忙看一下。相关配置及代码在压缩包。8054.CC2640R2F读取数据.7z
您好,我尝试使用RTC+GPIO中断来实现数据采集,您看下我下面使用的rtc时钟对吗?另外就是我想问一下AONRTCCaptureValueCh1Get()函数单位是秒吗?低16位代表的是毫秒(即1s均分为655535)?
//GPIO�궨�� #define DATA_GPIO IOID_26 #define CLK_GPIO IOID_27 //GPIO���ù��� PIN_Config GPIOConfig[] = { DATA_GPIO | PIN_GPIO_OUTPUT_DIS | PIN_INPUT_EN | PIN_PULLDOWN, CLK_GPIO | PIN_GPIO_OUTPUT_DIS| PIN_INPUT_EN | PIN_PULLUP, PIN_TERMINATE }; //�������� static PIN_State GPIOPinState; static PIN_Handle hGPIOPinsHandle; static u8 ClkNum = 0; //CLK�жϼ����� //�ڲ����ú��� static void CLK_GPIOIsrCallback(PIN_Handle handle, PIN_Id pinId); //------------------------------------------------------------------------------ //���� ���� void GPIO_Init(void) //���� ���� λ�Ƽ�GPIO��RTCʱ�ӳ�ʼ�� //����ڲ����� �� //�����ز����� �� //��˵ ���� �� //------------------------------------------------------------------------------ void GPIO_Init(void) { BleSDKManagerInfo_t err; // ״̬���� err = DriverIOOpen(&hGPIOPinsHandle,&GPIOPinState,(const PIN_Config *)GPIOConfig); //����IO���� if(err != MANAGER_INFO_REQUEST_IO_SUCCESS){ //һ��IO��ɹ� �����������û��IO return; } err = DriverIORegisterIntCallBack(&hGPIOPinsHandle,CLK_GPIOIsrCallback); //ע��һ��io�жϻص����� if(err != MANAGER_INFO_CONTROL_IO_SUCCESS){ return; } err = DriverIOSetConfig(&hGPIOPinsHandle,PIN_BM_IRQ,CLK_GPIO | PIN_IRQ_NEGEDGE);//����CLK_GPIO���жϹ��� if(err != MANAGER_INFO_CONTROL_IO_SUCCESS){ return; } #ifdef POWER_SAVING //���ϵͳ������ʡ�繦�� ����ҪΪ��io���û��ѹ���(��ʹ��߱���˯��״̬ͨ���жϻ���mcu�Ĺ���) err = DriverIOSetConfig(&hGPIOPinsHandle,PINCC26XX_BM_WAKEUP,CLK_GPIO | PINCC26XX_WAKEUP_NEGEDGE);//����CLK_GPIO���жϻ��ѹ��� if(err != MANAGER_INFO_CONTROL_IO_SUCCESS){ return; } #endif AONRTCChannelDisable(AON_RTC_CH1); AONRTCModeCh1Set(AON_RTC_MODE_CH1_CAPTURE); AONEventRtcSet(AON_EVENT_IO); AONRTCChannelEnable(AON_RTC_CH1); } //------------------------------------------------------------------------------ //���� ���� CLK_GPIOIsrCallback(PIN_Handle handle, PIN_Id pinId) //���� ���� io�жϻص����� //����ڲ����� �� //�����ز����� �� //��˵ ���� �� //------------------------------------------------------------------------------ static void CLK_GPIOIsrCallback(PIN_Handle handle, PIN_Id pinId) { static u32 uiDataTemp = 0; static u32 CLKedgeTimingCurrectValue[2] = {0}; u32 edgeTimingCurrectValue = 0; g_uiShutDownClk = 0; //shutdownģʽ��ʱ������ if(ClkNum == 0){ // CLKedgeTimingCurrectValue[0] = AONRTCCurrentCompareValueGet(); CLKedgeTimingCurrectValue[0] = AONRTCCaptureValueCh1Get(); AONRTCEventClear(AON_RTC_CH1); } else{ // CLKedgeTimingCurrectValue[1] = AONRTCCurrentCompareValueGet(); CLKedgeTimingCurrectValue[1] = AONRTCCaptureValueCh1Get(); AONRTCEventClear(AON_RTC_CH1); if(CLKedgeTimingCurrectValue[1] >= CLKedgeTimingCurrectValue[0]) edgeTimingCurrectValue = CLKedgeTimingCurrectValue[1] - CLKedgeTimingCurrectValue[0]; else edgeTimingCurrectValue = CLKedgeTimingCurrectValue[1] + (0xFFFFFFFF - CLKedgeTimingCurrectValue[0]); CLKedgeTimingCurrectValue[0] = CLKedgeTimingCurrectValue[1]; if(edgeTimingCurrectValue > 328){ //����5ms��5ms *(1000 / 65535) ClkNum = 0; uiDataTemp = 0; } } if(1 == DriverIOGetInputValue(DATA_GPIO)) //��ȡIO��ƽ uiDataTemp = uiDataTemp + (1 << ClkNum); ClkNum += 1; if(ClkNum >= 28){ //���ݶ�ȡ��� ClkNum = 0; g_uiData = uiDataTemp; g_cDataFinsh = 1; } }
您好,我在使用过程中发现:将断点打在if(ClkNum >= 28){}代码里面的ClkNum = 0;位置,程序是进不去的,一直进if(edgeTimingCurrectValue > 0x1000){}这个函数。进一步调试,将断点打在if(edgeTimingCurrectValue > 0x1000)处,edgeTimingCurrectValue的值很小,但是如果将断点打在if(edgeTimingCurrectValue > 0x1000)()函数里面的 ClkNum = 0处,edgeTimingCurrectValue值又会很大。请问是怎么回事?下面是中断处理函数的部分代码,具体整个文件的配置代码见文件
//GPIO�궨�� #define DATA_GPIO IOID_26 #define CLK_GPIO IOID_27 //GPIO���ù��� PIN_Config GPIOConfig[] = { DATA_GPIO | PIN_GPIO_OUTPUT_DIS | PIN_INPUT_EN | PIN_PULLDOWN, CLK_GPIO | PIN_GPIO_OUTPUT_DIS| PIN_INPUT_EN | PIN_PULLUP, PIN_TERMINATE }; //�������� static PIN_State GPIOPinState; static PIN_Handle hGPIOPinsHandle; static u8 ClkNum = 0; //CLK�жϼ����� //�ڲ����ú��� static void CLK_GPIOIsrCallback(PIN_Handle handle, PIN_Id pinId); //------------------------------------------------------------------------------ //���� ���� void GPIO_Init(void) //���� ���� λ�Ƽ�GPIO��RTCʱ�ӳ�ʼ�� //����ڲ����� �� //�����ز����� �� //��˵ ���� �� //------------------------------------------------------------------------------ void GPIO_Init(void) { BleSDKManagerInfo_t err; // ״̬���� err = DriverIOOpen(&hGPIOPinsHandle,&GPIOPinState,(const PIN_Config *)GPIOConfig); //����IO���� if(err != MANAGER_INFO_REQUEST_IO_SUCCESS){ //һ��IO��ɹ� �����������û��IO return; } err = DriverIORegisterIntCallBack(&hGPIOPinsHandle,CLK_GPIOIsrCallback); //ע��һ��io�жϻص����� if(err != MANAGER_INFO_CONTROL_IO_SUCCESS){ return; } err = DriverIOSetConfig(&hGPIOPinsHandle,PIN_BM_IRQ,CLK_GPIO | PIN_IRQ_NEGEDGE);//����CLK_GPIO���жϹ��� if(err != MANAGER_INFO_CONTROL_IO_SUCCESS){ return; } #ifdef POWER_SAVING //���ϵͳ������ʡ�繦�� ����ҪΪ��io���û��ѹ���(��ʹ��߱���˯��״̬ͨ���жϻ���mcu�Ĺ���) err = DriverIOSetConfig(&hGPIOPinsHandle,PINCC26XX_BM_WAKEUP,CLK_GPIO | PINCC26XX_WAKEUP_NEGEDGE);//����CLK_GPIO���жϻ��ѹ��� if(err != MANAGER_INFO_CONTROL_IO_SUCCESS){ return; } #endif AONRTCChannelDisable(AON_RTC_CH1); AONRTCModeCh1Set(AON_RTC_MODE_CH1_CAPTURE); AONEventRtcSet(AON_EVENT_IO); AONRTCChannelEnable(AON_RTC_CH1); } //------------------------------------------------------------------------------ //���� ���� CLK_GPIOIsrCallback(PIN_Handle handle, PIN_Id pinId) //���� ���� io�жϻص����� //����ڲ����� �� //�����ز����� �� //��˵ ���� �� //------------------------------------------------------------------------------ static void CLK_GPIOIsrCallback(PIN_Handle handle, PIN_Id pinId) { static u32 uiDataTemp = 0; static u32 CLKedgeTimingCurrectValue[2] = {0}; u32 edgeTimingCurrectValue = 0; g_uiShutDownClk = 0; //shutdownģʽ��ʱ������ if(ClkNum == 0){ // CLKedgeTimingCurrectValue[0] = AONRTCCurrentCompareValueGet(); CLKedgeTimingCurrectValue[0] = AONRTCCaptureValueCh1Get(); AONRTCEventClear(AON_RTC_CH1); } else{ // CLKedgeTimingCurrectValue[1] = AONRTCCurrentCompareValueGet(); CLKedgeTimingCurrectValue[1] = AONRTCCaptureValueCh1Get(); AONRTCEventClear(AON_RTC_CH1); if(CLKedgeTimingCurrectValue[1] >= CLKedgeTimingCurrectValue[0]) edgeTimingCurrectValue = CLKedgeTimingCurrectValue[1] - CLKedgeTimingCurrectValue[0]; else edgeTimingCurrectValue = CLKedgeTimingCurrectValue[1] + (0xFFFFFFFF - CLKedgeTimingCurrectValue[0]); CLKedgeTimingCurrectValue[0] = CLKedgeTimingCurrectValue[1]; if(edgeTimingCurrectValue > 328){ //����5ms��5ms *(1000 / 65535) ClkNum = 0; uiDataTemp = 0; } } if(1 == DriverIOGetInputValue(DATA_GPIO)) //��ȡIO��ƽ uiDataTemp = uiDataTemp + (1 << ClkNum); ClkNum += 1; if(ClkNum >= 28){ //���ݶ�ȡ��� ClkNum = 0; g_uiData = uiDataTemp; g_cDataFinsh = 1; } }
CLKedgeTimingCurrCLKedgeTimingCurrectValue[1] = AONRTCCaptureValueCh1Get();
AONRTCEventClear(AON_RTC_CH1);
if(CLKedgeTimingCurrectValue[1] >= CLKedgeTimingCurrectValue[0])
edgeTimingCurrectValue = CLKedgeTimingCurrectValue[1] - CLKedgeTimingCurrectValue[0];
else
edgeTimingCurrectValue = CLKedgeTimingCurrectValue[1] +(0xFFFFFFFF - CLKedgeTimingCurrectValue[0]);
if(edgeTimingCurrectValue > 0x1000){ //大约62ms
ClkNum = 0;
uiDataTemp = 0;
}
CLKedgeTimingCurrectValue[0] - CLKedgeTimingCurrectValue[1];
ClkNum += 1;
if(ClkNum >= 28){
ClkNum = 0;
.....
}