你好,TI技术员
使用官方例子,作为发射端时可以发射信号,作为接收端时去接收不到信号。是硬件电路的问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用: rfEasyLinkRx rfEasyLinkTx这两个例程,有两块板子A和B,当A下载发射程序,B下载接收程序时,A能发射正确信号,B能接收正确信号;当A下载接收程序,B下载发送程序时,B可以发射信号,但A去接收不到信号。供电电压3.3V,DCDC_SW输出1.67V,CC1310F128芯片QFN48封装
user4333850 说:你好,我还想请教下,CC1310对24MHZ的晶振有什么要求?前后购买两次24M晶振,后面购买的就用不了,焊到别的MCU上去测试,频率也是24M,
规格书里面有对于24MHz crystal的需求。你在采购的时候,需要标定负载电容的。
BR.AZ