CC1352P 在433M能否使用内置PA 发射功率能达到20dBm吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC1352P 在433M能否使用内置PA 发射功率能达到20dBm吗?
Chance,
可以的。但任何一个允许433MHz ISM频段的国家的无线电认证都不能达到这个功率的。所以并没有声称。
我帮你确认一下在这个频段下的效率问题。回头反馈。
如果其他433MHz的参考设计方案,请参考置顶帖https://e2echina.ti.com/question_answer/wireless_connectivity/hw_rf_proprietary/f/45/t/124625
BR. AZ
Chance1 说:好的,非常感谢,期待你的回复。
Chance,
可以支持的,特别是电流才55mA。这个很好哦。
如果你看我用SKY PA做的那个参考设计,电流要将近80mA呢。
BR. AZ