This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求救,急需cc1310配置高速模式的方法,1M-2M都可以

Other Parts Discussed in Thread: CC1310, CC1350

求救,急需cc1310配置高速模式的方法,1M-2M都可以 谢谢

  • 高速通信的话,建议参考 rfPacketErrorRate,SDK里已包含
  • 最新版sdk里的rfPacketErrorRate支持到4Mbps

    Packet Error Rate Example Application

    The Packet Error Rate (PER) example showcases different RF transfer modes of the CC13xx and CC2640R2. It combines tasks, events and several peripherals to a platform- independent application and runs on all CC13xx and CC2640R2 launchpads as well as the CC1310EM/SmartRF06.

    Test cases are provided for the following RF modes:

    Custom: Custom settings to be exported from SmartRF Studio to the smartrf_settings.c file

    2-GFSK: Generic frequency shift keying with binary symbols, 50 kBit/s for all launchpads, 250 KBits/s for the CC2640R2

    LR Mode: Legacy Long Range (625 bps)

    OOK: On-off keying

    HS Mode: High-speed mode with up to 4 MBit/s

    SL LR: SimpleLink Long Rang (5 kbps)

    BLE: Bluetooth Low Energy (CC135X, CC2640R2 only)

    BLE5: Bluetooth Low Energy 5 (CC1352, CC2640R2 only)

    Note that

    HSM and OOK are not supported on the CC1310-CC1190, CC1350 (433 MHz), CC1352 (R1/P1/P-2/P-4) or CC2640R2 Launchpads

    Legacy Long Range Mode (LRM) is not supported on the CC1352(R1/P1/P-2/P-4).

    你是用的官方的板子,还是自己的板子呢。官方板子的话是不支持HSM and OOK are not supported on the CC1310-CC1190 Launchpads的。