If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Packet Error Rate (PER) example showcases different RF transfer modes of the CC13xx and CC2640R2. It combines tasks, events and several peripherals to a platform- independent application and runs on all CC13xx and CC2640R2 launchpads as well as the CC1310EM/SmartRF06.
Test cases are provided for the following RF modes:
Custom: Custom settings to be exported from SmartRF Studio to the smartrf_settings.c file
2-GFSK: Generic frequency shift keying with binary symbols, 50 kBit/s for all launchpads, 250 KBits/s for the CC2640R2
LR Mode: Legacy Long Range (625 bps)
OOK: On-off keying
HS Mode: High-speed mode with up to 4 MBit/s
SL LR: SimpleLink Long Rang (5 kbps)
BLE: Bluetooth Low Energy (CC135X, CC2640R2 only)
BLE5: Bluetooth Low Energy 5 (CC1352, CC2640R2 only)
Note that
HSM and OOK are not supported on the CC1310-CC1190, CC1350 (433 MHz), CC1352 (R1/P1/P-2/P-4) or CC2640R2 Launchpads
Legacy Long Range Mode (LRM) is not supported on the CC1352(R1/P1/P-2/P-4).
你是用的官方的板子,还是自己的板子呢。官方板子的话是不支持HSM and OOK are not supported on the CC1310-CC1190 Launchpads的。