大家好,
请问在CC1310中如何实现把一个字节数据写入到指定的flash地址中呢?
类似msp430功能实现:
unsigned long * Flash_ptrC; // Initialize Flash pointer Seg D unsigned long tmp; tmp = value; Flash_ptrC = (unsigned long *) 0x1880; // Initialize Flash pointer FCTL3 = FWKEY; // Clear Lock bit FCTL1 = FWKEY+ERASE; // Set Erase bit *Flash_ptrC = 0; // Dummy write to erase Flash seg while(FCTL3&BUSY); FCTL1 = FWKEY+BLKWRT; // Enable long-word write *Flash_ptrC = tmp; // Write to Flash while(FCTL3&BUSY); FCTL1 = FWKEY; // Clear WRT bit FCTL3 = FWKEY+LOCK;
希望能尽快得到帮助!
谢谢!