This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

smartrf studio的continuous TX和parket TX区别

用continuous TX发数据,用频谱仪可以看到一个很好很完整的波形,但是用parket TX发数据,用频谱仪只能看到时有时无的脉冲,而且是在中心频点的周围。

因此,我想问的是,

(1)所谓的持续发射的模式和parket TX模式,到底有什么区别?

(2)是不是说发包时间间隔的差别,如果真的是这个差别,请问,两种发射模式的发送数据的间隔是多少

  • -Continuous TX for transmitting an un-modulated or modulated carrier. Also
    possible to set up frequency sweeps, which can be useful for measuring antenna
    bandwidth.Continuous RX for testing radiation in RX and for simple scanning of energy
    level on the given frequency.

    用于发送未调制或调制的载波的连续发送。

    可设置频率扫描,可用于测量天线带宽。

    parket TX: 是个一个完整的数据包 测试误码率和丢包率。