之前测试没问题的设备,现在接收时出现EasyLink_Status_Aborted的错误,可能是什么原因导致的?
SDK:simplelink_cc13x2_26x2_sdk_3_40_00_02
IAR:8.50.4
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前测试没问题的设备,现在接收时出现EasyLink_Status_Aborted的错误,可能是什么原因导致的?
SDK:simplelink_cc13x2_26x2_sdk_3_40_00_02
IAR:8.50.4
** * @brief Runs synchronously an RF operation command or a chain of commands and returns * the termination reason. * * This function appends an RF operation command or a chain of commands to the RF driver's * command queue and then waits for it to complete. * A command is completed if one of the termination events ::RF_EventLastCmdDone, * ::RF_EventCmdCancelled, ::RF_EventCmdAborted, ::RF_EventCmdStopped occurred. * * This function is a combination of RF_postCmd() and RF_pendCmd(). * All options and limitations for RF_postCmd() apply here as well. * * An application should always ensure that the command completed in the expected way and * with an expected status code. * * @note Calling context : Task * * @param h Driver handle previously returned by RF_open() * @param pOp Pointer to the RF operation command. * @param ePri Priority of this RF command (used for arbitration in multi-client systems) * @param pCb Callback function called during command execution and upon completion. * If RF_runCmd() fails, no callback is made. * @param bmEvent Bitmask of events that will trigger the callback or that can be pended on. * @return The relevant termination event. * * @sa RF_postCmd(), RF_pendCmd(), RF_cancelCmd(), RF_flushCmd() */ extern RF_EventMask RF_runCmd(RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent);
看起来像是是射频部分的问题,检查下这部分