CC3200 LaunchPad 剛開始使用時在 "Code Composer Studio 6.0.1" 與 "CCS UniFlash" 燒錄程序與flash都正常,但是使用幾次之後,目前都出現下載程序與燒錄Flash 時都是失敗的狀況,請問是哪出了問題?
绝对不是硬件连接问题,串口选择等问题,我认为是3200某个设计问题,希望ti的大神们使用3200的遇到过这种问题的工程师来解答一下,很很急
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
[20:26:47] Begin Program operation. [20:26:48] INFO: > Executing Operation: Connect [20:26:50] INFO: setting break signal [20:26:51] INFO: detecting FTDI for device reset [20:27:06] ERROR: ---reading ACK signal failed--- [20:27:06] WARNING: ---seting break signal to false failed--- [20:27:08] INFO: setting break signal [20:27:09] INFO: detecting FTDI for device reset [20:27:25] ERROR: ---reading ACK signal failed--- [20:27:25] WARNING: ---seting break signal to false failed--- [20:27:27] INFO: setting break signal [20:27:28] INFO: detecting FTDI for device reset [20:27:43] ERROR: ---reading ACK signal failed--- [20:27:43] WARNING: ---seting break signal to false failed--- [20:27:45] INFO: setting break signal [20:27:46] INFO: detecting FTDI for device reset [20:28:02] ERROR: ---reading ACK signal failed--- [20:28:02] WARNING: ---seting break signal to false failed--- [20:28:02] FATAL: --- Can't connect to device !! --- [20:28:02] FATAL: Error connecting to the device. Please check your COM port settings. Error code: -3 [20:28:02] INFO: > Executing Operation: Disconnect [20:28:02] Operation Program returned.
这是软件部分
这是软件设置
首先保证USB转串口FT部分是可以正常工作的,在下载过程中如果提示要进行Device reset时,需要手动进行复位,或者直接更新最新的Uniflash进行下载工作。
硬件板卡检查SOP的设置,将SOP设置为100,即SOP2上拉,其余两个保持低电平状态,此时CC3200启动后进入了UART0模式,进行程序的烧录工作。