This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

那位前辈有64位的win10系统的ccs6.0开发平台

Other Parts Discussed in Thread: CC3200, CC2650, CC2538, ENERGIA, ENERGYTRACE

那位前辈有64位的win10系统的ccs6.0开发平台,我是新手,电脑是64位的win10系统,想学习cc3200的芯片,但是没有开发平台,谢谢

  • 如下link下载,想要什么版本自己挑

    http://processors.wiki.ti.com/index.php/Download_CCS

    Code Composer Studio Version 6 Downloads

    It is highly recommended to use the latest version of Code Composer Studio as patches are not provided for older versions.

    There are two types of installers:

    • Web installers will allow you to perform an install using an installer controlled download process that will only download needed software components. An internet connection is mandatory at install time.
    • Off-line installers are a large archive (about 730MB). When you run it you can select the components to be installed. No internet connection is required at install time. The executable can be used for installing multiple local systems.

    If you have an issue with the web installer not being able to connect to the internet then please try the off-line installer. If you need to update a computer that does not have internet access then download the offline installer and then transfer it to the computer without access and use the offline installer to update your installation.

    Release Build # Date Download Notes
    6.2.0 6.2.0.00050 Sept 14, 2016 Web Installers:
    Windows
    Linux - 64-bit only

    MacOS

    Off-line Installers:
    Windows MD5 
    Linux MD5 - 64-bit only 
    MacOS MD5 

    • New in this release:
    • Release notes
    • Build 50 vs 48
    • Bug fixes for flashing issues on Connectivity devices
    • Resource Explorer bug fixes and startup performance improvements
    • Installation: see instructions in README Linux file. See also additional Linux Installation Instructions
    • The manifest lists the software components included in this product.
    • Update Status: this release will not be available as an update.
    6.2.0 6.2.0.00048 Aug 31, 2016 Web Installers:
    Windows
    Linux - 64-bit only

    MacOS

    Off-line Installers:
    Windows MD5 
    Linux MD5 - 64-bit only 
    MacOS MD5 

    • New in this release:
    • Release notes
    • Support for MacOS (CC13xx, CC2538, CC2650, CC3200, C2000, MSP430, MSP432, TM4C, Hercules)
    • Bug fixes
    • Updated device support
    • Eclipse 4.5
    • ARM, C2000, MSP430 compiler update to 15.12.3 LTS
    • Resource Explorer v2.0 BETA
    • Installation: see instructions in README Linux file. See also additional Linux Installation Instructions
    • The manifest lists the software components included in this product.
    • Update Status: this release will not be available as an update.
    6.1.3 6.1.3.00034 Jul 2, 2016 Web Installers:
    Windows
    Linux

    MacOS

    Off-line Installers:
    Windows MD5 
    Linux MD5 
    MacOS MD5 

    • New in this release:
    • Support for MacOS (CC13xx, CC2538, CC2650, CC3200, C2000, MSP430, MSP432, TM4C, Hercules)
    • Bug fixes
    • Updated device support
    • Eclipse 4.5
    • ARM, C2000, MSP430 compiler update to 15.12 LTS
    • Build 33 vs 34 There is no functional difference between build 33 and 34, the only change was to correct an issue in the installer.
    • Installation: see instructions in README Linux file. See also additional Linux Installation Instructions
    • The manifest lists the software components included in this product.
    • Update Status: this release will not be available as an update.
    6.1.3 6.1.3.00033 Apr 22, 2016 Web Installers:
    Windows
    Linux

    MacOS

    Off-line Installers:
    Windows MD5 
    Linux MD5 
    MacOS MD5 

    • New in this release:
    • Support for MacOS (CC13xx, CC2538, CC2650, CC3200, C2000, MSP430, MSP432, TM4C, Hercules)
    • Bug fixes
    • Energia 17 support
    • Updated device support
    • Eclipse 4.5
    • ARM, C2000, MSP430 compiler update to 15.12 LTS
    • Build 33 vs 34 There is no functional difference between build 33 and 34, the only change was to correct an issue in the installer.
    • Installation: see instructions in README Linux file. See also additional Linux Installation Instructions
    • The manifest lists the software components included in this product.
    • Update Status: this release will not be available as an update.
    6.1.2 6.1.2.00015 Dec 23, 2015 Web Installers:
    Windows
    Linux


    Off-line Installers:
    Windows MD5 
    Linux MD5 

    • New in this release:
    • Bug fixes
    • Updates to KeyStone device support
    • Updates to Sitara device support
    • C6000 8.1 Compiler
    • Update Status: this release will not be available as an update.
    6.1.1 6.1.1.00022 Sept 16, 2015 Web Installers:
    Windows
    Linux


    Off-line Installers:
    Windows MD5 
    Linux MD5 

    • New in this release:
    • Updates to SimpleLink CC26xx and CC13xx Wireless Connectivity MCUs
    • XDS110 automatic firmware update
    • CC3200 support on Linux
    • DRA7x support
    • Energia 15 and 16 support
    • Bug fixes.
    • Installation: see instructions in README Linux file. See also additional Linux Installation Instructions
    • The manifest lists the software components included in this product.
    • If you wish to update a previous install then please install the update from within CCS instead of downloading this installation and pointing it to your existing install.
    6.1.0 6.1.0.00104 Feb 25, 2015 Web Installers:
    Windows
    Linux


    Off-line Installers:
    Windows MD5 
    Linux MD5 

    • New in this release:
    • Enhancements to IDE:
      • Integration with Eclipse v4.4.1 and CDT 8.3.
    • Added support for SimpleLink™ CC26xx and CC13xx MCU platform of devices.
    • Added support for on-board USB XDS110 debug (Hercules RM46x Launchpad).
    • Support for GCC for MSP430.
    • MSP EnergyTrace
      • Improved EnergyTrace tool for profiling application’s energy consumption, battery lifetime, monitoring internal device states and determining execution hotspots (statistical function profile)
    • Energia 14 support
    • Bug fixes.
    • Installation: see instructions in README Linux file. See also additional Linux Installation Instructions
    • The manifest lists the software components included in this product.
    • If you wish to update a previous install then please install the update from within CCS instead of downloading this installation and pointing it to your existing install.
    6.0.1 6.0.1.00040 Aug 3, 2014 Web Installers:
    Windows
    Linux


    Off-line Installers:
    Windows MD5 
    Linux MD5 

    • New in this release:
      • Fixes an installation issue for laptops using NVidia Optimus-based graphics controllers. No other content changes.
    • Installation: see instructions in README file. Additional Linux Installation Instructions
    • The software manifest lists the software components included in this product.
    • If you wish to update a previous install then please install the update from within CCS instead of downloading this installation and pointing it to your existing install.
    6.0.1 6.0.1.00039 July 22, 2014 Web Installers:
    Windows
    Linux


    Off-line Installers:
    Windows MD5 
    Linux MD5 

    • New in this release:
      • Support for Hercules RM57L and TMS570LC (Cortex-R5/R5F)
      • Support for SimpleLink CC32xx (Windows only).
      • New MSP430 EnergyTrace tool for profiling application’s energy consumption, monitoring internal device states and determining execution hotspots (statistical function profile)
      • Energia 13 support.
    • Installation: see instructions in README file. Additional Linux Installation Instructions
    • The software manifest lists the software components included in this product.
    • If you wish to update a previous install then please install the update from within CCS instead of downloading this installation and pointing it to your existing install.
    6.0.0 6.0.0.00190 April 21, 2014 Web Installers:
    Windows
    Linux


    Off-line Installers:
    Windows MD5 
    Linux MD5 

    • New in this release: App Center, Getting Started View, Simple Mode, Eclipse 4.3, Energia 12 support.
    • Installation: see instructions in README file. Additinal Linux Installation Instructions
    • The software manifest lists the software components included in this product.

  • 那请问一下,如何知道下载的安装包是64位的

  • 自版本CCSv6.1.3以上,都是支持win10 64-bit的
  • 可以下载8.0的了。