This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100MODBOOST使用时遇到问题

Other Parts Discussed in Thread: CC3100MODBOOST, CC3100SDK, CC3100

请求大神指点迷津!!!

1.硬件环境:

CC3100MODBOOST(rev1.0) + AVR ATxmega128B1(SPI接口)

2.调试环境:

Atmel studio 7.0,代码采用C:\TI\CC3100SDK\cc3100-sdk\examples\tcp_socket

3.调试过程:

(1)使用CC3100SDK0.5.1版:CC3100作为客户端,NetAssist设置为服务端。

运行程序,设置断点。

现象1:若NetAssist向CC3100发送10个数据包,发送间隔长时(大约3秒),发送完毕后,可以正常关闭SOCKET,发送间隔小的话,程序始终在_SlNonOsMainLoopTask中循环。

现象2:若CC3100向NetAssist发送10个数据包,NetAssist只收到一个数据包,程序始终在_SlNonOsMainLoopTask中循环,运行不到断点。

下图为NetAssist和wirshark 抓的数据包。

 

 

(2)使用CC3100SDK0.5.1版:CC3100作为服务端,NetAssist设置为客户端(NO_OF_PACKETS定义为10),

运行程序,

现象1:NetAssist向CC3100发送10个数据包,发送完毕后关闭SOCKET都正常。

现象2:若CC3100向NetAssist发送10个数据包,NetAssist只收到一个数据包,程序始终在_SlNonOsMainLoopTask中循环。

下图为NetAssist和wirshark 抓包。

 

4.首先怀疑是SPI接口驱动移植有问题,于是用CC3100SDK_1.3.0版中spi_debug_tool进行测试,测试正常,如图示:

 

是哪里出了问题呢?