This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 烧录/sys/mcuimg.bin 文件时,使用CCS UniFlash 烧录时 提示ERROR: Open operation failed

Other Parts Discussed in Thread: UNIFLASH, CC3200

如题,CC3200 烧录/sys/mcuimg.bin 文件时,使用CCS UniFlash 烧录时,提示ERROR: Open operation failed,但bin文件如果小一点又可以烧录进去,而且程序正常运行,说明flash的读取是没问题的,唯一区别就是 bin文件过大(原来160K,大一点170K)就提示R: Open operation failed,之前怀疑是FLASH大小不够,由1M换成2M,仍然出现该问题,请工程师们解答一下呢,谢谢

  • uniflash的完整log请提供一下
  • 确认一下,再烧录bin文件之前,有没有先格式化再操作?
  • 没有先格式化,因为除了/sys/mcuimg.bin,还有其他的一些网页文件,所以我是以替换/sys/mcuimg.bin方式进行的,这个是不是存在问题呢,问题是出在哪里呢?
    这是出错的日志
    [16:08:27] Begin Program operation.
    [16:08:28] INFO: > Executing Operation: Connect
    [16:08:30] INFO: setting break signal
    [16:08:31] INFO: detecting FTDI for device reset
    [16:08:31] ERROR: No device USB ports were found
    [16:08:31] INFO: --- please restart the device ---
    [16:08:40] INFO: connection succeeded
    [16:08:40] INFO: getting storage list
    [16:08:40] INFO: > Executing Operation: Init
    [16:08:40] INFO: reading version info
    [16:08:40] INFO: DEVICE CC3200 ES1.33
    [16:08:40] INFO: reading version info
    [16:08:41] INFO: reading version info
    [16:08:43] INFO: > Executing Operation: Program
    [16:08:43] INFO: > File name: /sys/mcuimg.bin, Update: true, Erase: true
    [16:08:43] INFO: > Erase File: /sys/mcuimg.bin
    [16:08:43] INFO: erasing file "/sys/mcuimg.bin"
    [16:08:43] INFO: deleting file "/sys/mcuimg.bin"
    [16:08:43] INFO: erase file completed
    [16:08:43] INFO: > Size of file = 176784
    [16:08:43] INFO: > Update File: /sys/mcuimg.bin
    [16:08:43] INFO: Downloading file "/sys/mcuimg.bin" with size 176784
    [16:08:43] ERROR: Open operation failed
    [16:08:43] INFO: > Executing Operation: Disconnect
    [16:08:43] Operation Program returned.
  • 就是没有格式化引起的问题,烧录之前需要格式化,网页文件可以后续通过application binary再烧录进去