你好:
我们的一款产品用了cc3220sf这个芯片,用的过程中出现了问题,现在系统启动不起来,我们换了单片机及外接flash,还是不能下载程序,我们排错的过程中发现单片机的9、36、42脚的电压为0,请问在单片机没有程序运行的情况下,只是供电,这几个引脚会有电压吗?另外不能下载程序可能有哪些原因呢?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
板子是自己制作的还是launchpad?用Uniflash可以识别吗,不能下载出现的具体错误是什么,
9、36、42引脚都是通过电容接到GND的,关于电路部分可以看下原理图:www.ti.com.cn/.../CC3220SF-LAUNCHXL
板子是自己做的,不是开发板,uniflash不接我自己的板子,只接下载器也能显示出cc3220sf,9、36、42脚是dcdc的输出,是给单片机的数字模拟和射频部分供电的,不是接地的,我们另一块正常的板子这三个脚都有电压输出的。下载时就卡在connect这里,总是连接不上,显示错误为超时。