SimpleLink™ Wi Fi® Starter Pro_v2.2.22_apkpure.com.apk , google play下不了的可以到这里!

榜眼 39027 points

https://apkpure.com/simplelink%E2%84%A2-wi-fi%C2%AE-starter-pro/com.ti.smartconfig

SimpleLink™ Wi-Fi® Starter Pro icon

SimpleLink™ Wi-Fi® Starter Pro APK

The description of SimpleLink™ Wi-Fi® Starter Pro

The SimpleLink™ Wi-Fi® Solution Starter Pro mobile app is a tool for users to configure, connect and communicate with TI's CC31xx and CC32xx devices. 
• Configure the SimpleLink Wi-Fi device to connect to an access point
• Locate other SimpleLink Wi-Fi devices connected to the network

The SimpleLink Wi-Fi family is the first in a series of easy to use, low power wireless connectivity solutions for the IoT. This Wi-Fi CERTIFIED™ chips and modules allow customers to easily add embedded Wi-Fi and Internet connectivity to a wide-range of home, industrial and consumer electronics.
• SimpleLink Wi-Fi CC31xx: Connect any microcontroller (MCU) to the Internet of Things with this wireless network processor 
• SimpleLink Wi-Fi CC32xx: Industry's first single-chip Wi-Fi solution with user-dedicated programmable MCU

For more information on the SimpleLink Wi-Fi family, or to download the latest host embedded code, visit: www.ti.com/simplelinkwifi
Show less

What's new

2017-02-25
- Bug fixes

www.deyisupport.com

 

3 个回复