This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
支持
• Enable/Disable 5-GHz Channels
For CC3235S and CC3235SF devices, this setting enables or disables 5-GHz channels in STA mode.
By default, 5-GHz channels are enabled in the system and the scanning time might be longer due to
the total number of enabled channels. In deployments that do not use these channels, disabling the
channels might improve the scan time and power consumption.
The mode can be changed by setting 0 to disable 5-GHz channels and 1 to enable.
Example:
_i16 Status;
_u8 Mode = 0; //0 disable 5GHz mode
Status = sl_WlanSet(SL_WLAN_CFG_GENERAL_PARAM_ID, WLAN_GENERAL_PARAM_OPT_ENABLE_5G, 1, (_u8
*)&Mode);
if( Status )
{
/* error */
}