This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630烧写程序时无法识别芯片

Other Parts Discussed in Thread: CC2630, CC2650EM-4XS-RD, CC2650

现在使用4x4mm封装的CC2630RSM芯片搭建一个低功耗的zigbee无线网络。想使用它功耗最低、外电路最简单的Single ended operation模式进行射频通信,目前做了一套板子。供电方式使用的是Internal DC-DC regulator,原理图如下图所示,附件有PDF格式的原理图。

软件使用IAR和TI的smartRF flash Program2.下载工具使用XDS100V3和jlink,接口使用TMS,TCK,RESET,VCC,GND的JTAG接线方式,其中Jlink和XDS100V3驱动安装正常。

目前iar搭配XDS100V3和iar搭配jlink皆已经验证无法下载程序。目前判断为硬件板子问题,但无法判断具体引起的原因。使用xds和flash program2下载程序时截图如下所示,能够识别下载器,但是无法识别CC2630芯片。

目前已经尝试过的方法是:更换VDDS_DCDC电容为10uF,以及多焊接了几块板子排除焊接错误。但是仍旧无法识别芯片进行程序烧写,请问各位大大这是哪里出了问题?十分感谢!

cc2630 - 核心.pdf