void ZDO_ProcessDeviceAnnce( zdoIncomingMsg_t *inMsg )中的一段代码:
if ( ZSTACK_ROUTER_BUILD ) { // If the device annce comes from a end device child that has moved // to another parent, remove it from associated device list // If the dev annce is coming from other device's children, // (The dev annce from its own children shall be unicast to itself, // So check the mac destination address) // Remove it from the associated device list. If it is not // a child, no action will be taken in AssocRemove() anyway. if ( inMsg->macDestAddr != NLME_GetShortAddr() ) { associated_devices_t *dev_ptr; // If it's an end device child dev_ptr = AssocGetWithExt( Annce.extAddr ); if ( dev_ptr ) { if ( dev_ptr->nodeRelation == CHILD_RFD || dev_ptr->nodeRelation == CHILD_RFD_RX_IDLE ) { AssocRemove( Annce.extAddr ); } } // Remove the address from the SrcMatch table, // just in case the device was aged out by Child Management Table process if ( ( pNwkNotMyChildListDelete != NULL ) && ( zgChildAgingEnable == TRUE ) ) { pNwkNotMyChildListDelete( Annce.nwkAddr ); } } }
代码中的注释:
// (The dev annce from its own children shall be unicast to itself,
// So check the mac destination address)
可以单播?
抓包发现Device Announce都是广播的,那么AssocRemove( Annce.extAddr );将会执行,即删除关联表。