终端节点和协调器建立连接过程中,协调器像是死机没有反应。附件为抓包文件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对原始例程仅仅加了开关控制功能,按理说和代码关系不大,并且节点烧录路由器代码的话是没有问题的,就是烧录终端代码就会出现协调器响应很慢甚至没有响应的现象。路由器代码和终端代码是一套代码。
我用了新的协议栈代码,编译协调器出错
Error[e16]: Segment XDATA_Z (size: 0x1e22 align: 0) is too long for segment definition. At least 0x723 more bytes needed. The problem occurred while processing the segment placement command
我调整XDATA到0x800也不起作用
SECURE=1
TC_LINKKEY_JOIN
NV_INIT
NV_RESTORE
xZTOOL_P1
xMT_TASK
xMT_APP_FUNC
xMT_SYS_FUNC
xMT_ZDO_FUNC
xMT_ZDO_MGMT
xMT_APP_CNF_FUNC
LEGACY_LCD_DEBUG
LCD_SUPPORTED=DEBUG
MULTICAST_ENABLED=FALSE
ZCL_READ
ZCL_WRITE
ZCL_BASIC
ZCL_IDENTIFY
ZCL_SCENES
ZCL_GROUPS
ZCL_ON_OFF
MT_TASK
ZTOOL_P1
ZCL_REPORT_DESTINATION_DEVICE
ZCL_LEVEL_CTRL
1.请问我用cc2538做协调器,节点用cc2530,协议栈用zstack 3.0.2可以吗?
2.感觉3.0.2是不是太耗内存了,我优化代码后在cc2530上面还是跑不起来,该怎么办?
1. 可以
2. 建議你換CC2652R,或是用CC2538也行