Part Number: TPS92391 Dears, Could you confirm this circuit diagram?
/cfs-file/__key/communityserver-discussions-components-files/24/TPS92391.pdf The total current of the applied LED is 350mA.
Are the following two ways of use feasible? 1. Set LED_Set to…
Part Number: AWR2243BOOST Other Parts Discussed in Thread: AWR2243 , , UNIFLASH , MMWAVE-MCUPLUS-SDK , AWR1243BOOST , AWR1243 使用uniflash V8.6下载mmwave_dfp_02_02_04_00\mmwave_dfp_02_02_04_00\firmware包中的xwr22xx_mss_rprc.bin和xwr2xxx_radarss_rprc.bin作为固件烧录到AWR2243Boost的板载Flash中…
Part Number: IWR6843ISK Other Parts Discussed in Thread: IWR6843 , 第六步RF Power-up后出现报错
[09:41:52] [RadarAPI]: ar1.RfEnable() [09:42:08] Status: Failed, Error Type: RESP TIMEOUT [09:42:12] BSS Power Up async event was not received!
以下为全部配置日历:
[09:41:04] …
Part Number: MMWCAS-DSP-EVM Other Parts Discussed in Thread: MMWCAS-RF-EVM TI技术支持的工程师们你们好,我在使用MMWCAS-DSP-EVM以及MMWCAS-RF-EVM板的时候,用mmwavestudio上位机进行雷达数据的采集,使用的是官方提供的Cascade_Configuration_MIMO_Test.lua脚本进行硬件参数配置,配置成功之后利用Cascade_Capture.lua脚本进行雷达数据的采集测试。但是发现无法采集到数据…
Part Number: TPS65145 Other Parts Discussed in Thread: DLPC6540 TI的工程师 你好
我在使用TPS65145时,发现以下故障:上电后,TPS65145的使能信号出现一段时间的抖动(确定该抖动不是来自上一级输出端DLPC6540),之后该芯片输出异常,电压跌落;
第一次试产没有该问题,第二次试产出现3片该问题的板子;以下是示波器的测试图片,以及使用芯片的丝印,附件是设计的原理图,以及TI官网的参考设计图。
期待您尽快支持和答复。
TPS65145_DMD_Vbais…
Part Number: TDA4VM We are facing some issues while trying to replace the default demo application(mcusw->mcuss_demos->profiling->can or mcusw->mcuss_demos->profiling->cddipc) embedded in `tispl.bin` with another fw from SDK 9.0 (ti-processor…
Part Number: BQ34Z100-G1 Other Parts Discussed in Thread: GPCCHEM 您好,TI工程师
我按照这个流程学习成功后,直接在Data Memory修改Cycle Count 0,Update Status 02,再Reset,IT_ENABLE;用4A电流充放电,电池放完电,等VOK清零后,FCC会比实际容量少200多mAh
4A-CHG-4A-DSG.xlsx 充放电日志
Data Menory.gg.csv GG文件:学习后又用4A充放循环…