Part Number: BQ40Z50-R2 Hi Ti members
CC (Bit 8): Charge_Controller_Enabled (R/W) 1 = Internal charge control enabled 0 = Internal charge control disabled (default)
电量计这个内部的充电控制功能,怎么理解?是指电池可以内部做逻辑来控制充电mos吗?有没有相关的专题讲解这个功能的资料?
您好,看起来是进入了ROM mode
It's possible for the enter "ROM mode" if the checksum stored doesn't match the checksum calculated after a reset. Do the following:
Send command 0x08 to execute FW
Check that the bq40z50-R1 FW is executing
Send command…