Part Number: BQ76200 这是14串电池原理图,67200直接驱动MOS管,MOS管并联,充电10个,放电10个,还有一个预充电
现在的问题是,芯片上电后,使能信号都为低电平,但是CHG,PCHG,DSG直接输出了电池电压BAT,即59.5V,1.输出信号CHG等的高电平就是BAT电压吗,2.看真值表,使能低电平,输出也应该是低电平,但是输出是高电平,是不是可以判定芯片损坏了,3.电池电压BAT最高可以到60.2V,选型有问题没,或者您这里有推荐的.4.原理图您看有没有明显的错误…
您好,非常抱歉回复晚了
What is the function of this circuit? Particularly C1. What is at CN1?
With this, I still would not expect much current to flow into the DSG_EN pin. If PACK is 60-V, there would be a ~50.9-V drop across R2 due to the D1 9.1-V Zener, which…
Part Number: BQ76952 Other Parts Discussed in Thread: BQ76200
Hi,准备设计一款具有并包输出功能电BMS,大致框图如附件,请帮忙这个设计是否能够正常运行。
基本需求如下:
1、电池组为13S,额定输出功率6000W(AFE决定选用bq76952)
2、增加一组并包MOS控制,暂定使用bq76200
3、PM+为副电池包正端
相关疑问点:
附件的框图是否可行?
并包的控制MOS方向是否合理?
在主电池包MOS(Q1、Q2)全部关断情况下是否能够正常驱动并包MOS…
Part Number: BQ76930 Other Parts Discussed in Thread: BQ78350 , BQ76200 , 7串电池组,用BQ76930+BQ78350+BQ76200方案,在组装时会出现2个现象:
1)BQ76930最第一串采样回路异常,即最低1串耗电明显偏大,测试采样回路电阻200Ω左右,相当于芯片管脚短路,经查焊接质量良好,无虚焊及连锡情况。
2)保护板与电池组连接后,BQ76930明显发热,2.5v输出电压1.3V左右,测试2.5V对GND阻抗30Ω…