Part Number: TMS320F28388D Other Parts Discussed in Thread: C2000WARE 你好,提前感谢您能回答,
我在使用基于C2000的F28388D,在simulink使用MBD编译过程中报错。
1. 首先,如下图,报错的内容是: Build process stopped at compile stage. Unable to find the following link-only objects that are specified in…
Part Number: TMS320F2800157 Other Parts Discussed in Thread: DRV8300 , DRV8323 q1:May I know that the only motor driver library file in the official case of f280015x is Flash_lib_HVKIT_3SC. Does this fit with drv8300? If not, which model does this library…
Part Number: TMS320F280039C Other Parts Discussed in Thread: C2000WARE , SYSCONFIG 1.我按照clb user guide 进行设置了,目前出现了以下问题,目前别的文件生成都正常,但是没有vcd文件,同时也没有simulation文件夹
2.编译的结果是
"C:\\ti\\ccs1240\\ccs\\utils\\bin\\gmake" -k -j 16 clean -O DEL /F "syscfg…
你好,参考下工程师的回复:
With AC input it works as a PFC input stage. It boosts the input volt to generate a higher DC bus volt and shapes the input current. This is average current mode control (ACMC) AC/DC boost.
But for DC input, it will be the same except that…
Part Number: TMS320F28335 Other Parts Discussed in Thread: C2000WARE C:\ti\c2000\C2000Ware_5_02_00_00\libraries\calibration\hrpwm\f2823x\lib 这个目录下有多种lib库,SFO_TI_Build_V5_fpu.lib带浮点,能同时测六个通道,SFO_TI_Build_fpu.lib只能测4个通道,这个在手册里有说明。但是SFO_TI_Build_V5B_fpu.lib和SFO_TI_Build_V5B…
感谢您对TI产品的关注! 关于你的咨询,IWR6843AOPEVM 不支持直接和DCA1000配合。 而xWR6843ISK和IWR6843ISK-ODS,支持和DCA1000直接配合。
mmWaveICBOOST你可以把它看作一个扩展接口的底座。 下面是它的功能。
1.2.5 MMWAVEICBOOST • Hosts starter kit using two 60-pin high-density (HD) connector for the high-speed ADC data over CSI…
参考下文档中的这段话,上图只是相关的测试结果:
Before coding the SPLL structure it is essential to simulate the behavior of the PLL for different conditions on the grid. Fixed-point processors are used, for their for lower cost in many grid tied converters. IQ Math is a convenient…