Part Number: TPS65145 Other Parts Discussed in Thread: DLPC6540 TI的工程师 你好
我在使用TPS65145时,发现以下故障:上电后,TPS65145的使能信号出现一段时间的抖动(确定该抖动不是来自上一级输出端DLPC6540),之后该芯片输出异常,电压跌落;
第一次试产没有该问题,第二次试产出现3片该问题的板子;以下是示波器的测试图片,以及使用芯片的丝印,附件是设计的原理图,以及TI官网的参考设计图。
期待您尽快支持和答复。
TPS65145_DMD_Vbais…
Part Number: DLP2010 Other Parts Discussed in Thread: DLPA100 , DLPA1000 , Hi Team,
My Customer is looking for the device 2503253-6 G4,QFP-80
unfortunately, I can't find any information about this device. Can you advise any information about this device (status…
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。 因此、使用 TeraTerm 的 Serial J102只显示了我发送的命令。 以下是一个会话的快照:
我认为另一个会话显示了错误(可能是 DMD 电源问题?):
Command 0x0 execution took 52 us (greater than allowed 50 ms)
Command 0x11 execution took 77 us (greater than…
Part Number: DLPC7540EVM Other Parts Discussed in Thread: DLPA100 , DLPC7540 , 您好,采用GUI调试DLPA100,设置fan_pwm占空比,但是测量不到对应的波形,风扇也不动作,请问是哪里的问题?
demo板中有tilt sensor 接口,有推荐厂家或者型号吗?