Part Number: CC2640R2L CCS启动调试点击运行之后,几十秒后连接断开,报错信息如下:
Cortex_M3_0: GEL Output: Memory Map Initialization Complete. Cortex_M3_0: GEL Output: Board Reset Complete. CS_DAP_0: Power Failure on Target CPU: (Error -180 @ 0x0) The controller has detected a target…
The code you've provided is written in C and appears to be a function named SPIReset, which takes an unsigned integer baseAdd as a parameter. This function seems to reset the SPI module by writing a value to the SPIGCR0 register.
The HWREG macro is…
I understand your confusion. The `HWREG` function is not a standard C function, but rather a macro or inline function typically defined in the header files provided by the manufacturer of the microcontroller or development board. It is often used to access…
我尝试过debug,但是每次当我进入shutdown时,便会断开debug, Cortex_M0P: JTAG Communication Error: (Error -615 @ 0x0) The target failed to see a correctly formatted SWD header. The connection to the target may be unreliable. Try lowering the TCLK setting before trying again…
Part Number: TMS320C6678 第一个问题:INTC模块的事件映射到CPU中断INT4-INT15这个过程怎么实现的,通过硬件还是软件?模块里面的INTMUX1-3寄存器负责完成中断事件选择,它是怎么完成把128个事件随机映射到12个CPU中断的呢?在下面这个文档中,有使用软件配置,是否是用这种手动配置方式完成映射呢 /cfs-file/__key/communityserver-discussions-components-files/120/7144.Configuring-Interrupts…
HI Shine,
1.现在我们板子的状态就是SPI0接口挂了一个nor flash,量测DSP的发给flash的clk,MOSI,CS都是正常的,就是flash给DSP的返回值是FF,这个现象会和我选择的flash有关吗?我的flash的型号是GD25S512MDYIGR,规格书在附件中,能帮忙看下吗?谢谢 GD25S512MDFIG.pdf
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。 /* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification…