Part Number: DS90UH928Q-Q1 Dear sirs,
我司目前收到車廠RFQ
其車機端是使用DS90UB681 .請問RX 端應該搭配TI哪一款 IC
在請提供資訊
謝謝
Dear Sirs,
Our company currently receives RFQ
The vehicle side uses DS90UB681. Which RX IC should be paired to this TX
Please provide information
Thanks …
Are you using UB954 des or UB960 des?
If UB954, have you made this modification in the device tree k3-j721e-fpdlink-sk-fusion ?
Please note UB954 is supported from SDK 9.1. Are you using the same?
Part Number: SK-TDA4VM Other Parts Discussed in Thread: DS90UB954-Q1EVM , , DS90UB954-Q1
sdk: ti-processor-sdk-linux-j7-evm-08_06_01_02
连接SK-TDA4VM与ds90ub954-Q1EVM:
使用ds90ub954-Q1EVM的J26连接到SK-TDA4VM的J24,ds90ub954-Q1EVM的J26已经填充零欧姆电阻,连接情况如下图:
并在sk-tda4v…
Part Number: DS90UB954-Q1 Other Parts Discussed in Thread: TDA4VM 我们将DS90UB954扣接到TDA4VM上,并同时给两者供电。在uEnv.txt中设置name_overlays=k3-j721e-edgeai-apps.dtbo k3-j721e-fpdlink-sk-fusion.dtbo k3-j721e-fpdlink-imx390-rcm-0-0.dtbo。打印kernel的时候显示 DS90UB954 failed。(由于我们的带解串器的摄像头还没到货…