Hi
见datasheet 第21页描述:9.1.6 Output Overvoltage Protection Because the LM3409/09HV controls a buck current regulator, there is no inherent need to provide output overvoltage protection. If the LED load is opened, the output voltage will only rise as high…
Part Number: TPS99000-Q1 Other Parts Discussed in Thread: LM3409 规格书: https://www.ti.com/lit/ds/symlink/tps99001-q1.pdf
规格书的 第67页是电源架构图,关于LM3409芯片的供电是6.5V。
问题1:请问能否单独改为12V给LM3409供电?
问题2:如果 LM3409的电源 单独 改为12V供电,那TPS99000需要做相关的调整吗?
以上问题请帮忙解答,谢
Part Number: LM3409 Other Parts Discussed in Thread: DLP5530Q1EVM 您好:
在DLP5530Q1EVM套件中,RGB三色LED的驱动控制电路LM3409,有几个问题需要咨询了解一下:
根据LM3409的datasheet,这个控制芯片电流可以达到5A,图1。但是在DLP5530Q1EVM的驱动板电路中,限流设置是8A,图2。
问题:
因为LED是PWM调光,按LM3409的限电流公式,如果限流8A,那么VDAC输出电压就是最大了,2V左右…