Other Parts Discussed in Thread: UCC2897A 各位老师好:
我参考TI官网上的PMP5426用UCC2897A做了个电源,36-72V输入,14V/10A输出,300K的频率。磁芯用的是TDK的PC44PQ2625,变比为9:6,其他器件均与PMP5426一样。满载效率>95%,但是空载测试数据为:36V 输入,静态电流为0.17A;48V输入,静态电流为0.13A;72V输入,静态电流为0.18A。与PMP5426的空载测试结果还是有一定距离的。调了有一段时间了…
Other Parts Discussed in Thread: UCC2897A 各位大神好:
参考TI网站上UCC2897A的一个应用例子PMP5426做了一个电源。变压器自己绕制,原边,副边,辅助绕组变比为6:4:4,其他器件值与PMP5426相同,但是贴了几块之后发现,有的板子可以正常工作,有的无输出,测量是2897AVDD引脚电压只有11.23V,即BAIS输出11.23v,几个板子都是11.23V左右,测量D4,D7,L2,C13均正常,找了好久没有发现问题.谁能给个建议,谢谢了。其中一块正常的板子在把2897A拆掉重新装上之后也成11…