Part Number: MMWCAS-RF-EVM
TI工程师您好,目前我们通过测量上图中的FMCW_CLKOUT/SYNCOUT(来自master芯片)和FMCW_SYNCIN(来自所有芯片)两个信号的功率,发现master芯片相差有20dBm,slave芯片相差有30dBm,请问出现这种情况的原因是什么?和PCB使用的材料有关吗?
具体测量数值如下图,其中板1测量正常,板2出现上述问题:
Part Number: CC1201 Does CC1201 supports 402-405MHz , so called ''MICS'' RF bands?
If not ,can you give me some advices and some sub-1G RF transceviers without MCU ,and those transceivers have eWOR likes CC1201,and can work on the 402…
Part Number: IWR6843ISK Other Parts Discussed in Thread: IWR6843 , 第六步RF Power-up后出现报错
[09:41:52] [RadarAPI]: ar1.RfEnable() [09:42:08] Status: Failed, Error Type: RESP TIMEOUT [09:42:12] BSS Power Up async event was not received!
以下为全部配置日历:
[09:41:04] …
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: MMWCAS-DSP-EVM , 官方的mmwave studio似乎只能离线采集数据,根据网上方法对PROCESSOR_SDK_RADAR_03_08_00_00进行修改可以实现数据实时显示,但似乎截获的dataarray是固定形式的,我是否能获取原始的回波数据而不是处理后的信号, 因为我需要对原始信号进行处理,而不是如得到这些图片的数据