Part Number: TDA4VM
hi ti
Consult camera image problem
platform:TDA4 j721e
PSDK:rtos:ti-processor-sdk-rtos-j721e-evm-08_01_00_13
linux: ti-processor-sdk-linux-j7-evm-08_01_00_07
We use your company's platform and SDK, and there is a small probability…
Part Number: TPA3223 *Test Conditions:
1.Power is provided to the DUT (Net_PVDD & Net_5VP) by the DC power supply.
2.AMP Output(CH_1 & CH_2) connect to Loads(8 ohm).
3.Audio Precision Output(GND) connect to DUT_GND.
4.Use Audio Precision(AP-525…
Hi,
I think that you should consider the fact that a resistor is connected between the terminal of the relays.
even if the value is around 47 this is quite small compared to MOhm values of the voltage divider at the op amp side.