Part Number: SK-TDA4VM Other Parts Discussed in Thread: TDA4VM SK-TDA4VM的开发板是仅支持linux的SDK吗,那么如何对MCU进行编程开发呢?
想用CCS对TDA4VM上的MCU进行编程的话,有官方库或者例程吗?比如想通过MCU控制CAN通信,可以实现吗?
Part Number: TDA4VM We are facing some issues while trying to replace the default demo application(mcusw->mcuss_demos->profiling->can or mcusw->mcuss_demos->profiling->cddipc) embedded in `tispl.bin` with another fw from SDK 9.0 (ti-processor…
Part Number: DS90UB960-Q1EVM Other Parts Discussed in Thread: SK-TDA4VM
DS90UB960-Q1EVM解串器板通过J1或J3 CSI接口连接到SK-TDA4VM的J24 CSI接口, 如下图所示 这种 Samtec cable 如何购买呢?
请参考下面的帖子。
The value 4 and 7 represents the node parameter index for the TIDL node.
If you see the node api of TIDL node,
tivxTIDLNode(vx_graph graph, vx_kernel kernel, vx_reference appParams[], vx_tensor input_tensors[], vx_tensor output_tensors[])
…
Part Number: SK-TDA4VM
hello. I am testing v4l2h264enc with the pipeline below.
It shows the log like below, and it doesn't work.
When I set the videotestsrc caps height=1072(1073, ..., 1079), it doesn't report error and works fine.
Another…