Part Number: DP83TD510E-EVM Other Parts Discussed in Thread: DP83TD510E , USB-2-MDIO 你好!
数据手册中DP83td510E支持SMI接口,我用自己的单片机可以读写一些寄存器(例如:0x0002,0x0003),但是读取0x0a85时,数据为0000。在USB-2-MDIO程序中,“Extended register” 处于“No”的情况下,数据也为0000.
“Extended…
Other Parts Discussed in Thread: TUSB1044RNQEVM , TUSB1104 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。 https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1306431/tusb1044rnqevm-i-want-to-use-2port-4lane-usb-communica…
Part Number: TLV320AIC3204EVM-K Hi,
I used the 3204EVM suite to debug and test AGC. I use the P23 interface in the suite for power supply, use external IC to provide MCLK, WCLK, BCLK, SDA, SCL through I2C change register, MIC input from IN1L, after AGC…
Part Number: AM3352 Other Parts Discussed in Thread: AM3359 硬件板卡: AM3359 BBB 和 AM3352 BBB(仅处理器区别)
软件环境: ti-processor-sdk-linux-am335x-evm-09.01.00.001 和 ti-processor-sdk-linux-am335x-evm-06.03.00.106
场景:
A. 使用ti-processor-sdk-linux-am335x-evm-09.01.00…
TXU0304 好像还不能兼容你现在的原理图应用,因为它是固定方向的,只有第4通道是从B端到A端,因此只能应用于MISO,而在你的应用中MISO是在第2通道。
没有其他方案推荐给你了,换方案的话,建议查看下面FAQ:
[FAQ] Are there voltage level translation / level shifter device recommendations for the industry standard interfaces like GPIO, SPI, UART, I2C…
感谢您对TI产品的关注! 关于你的咨询, 1. BQ25756EVM是基于BQ25756推荐电路设计的,是支持评价BQ25756的反向功能的。 2. BQ25756的反向模式也是支持电压,电流调节。 The device supports buck-boost reverse power direction to deliver power from the battery to the input when the adapter is not present. In reverse mode, the…