Part Number: TMS320F28035 How do I make the DSP28035 (or any other model) get a three-way Hall signal?
The DSP28035 Ecap input port is only 1, and the single brushless motor Hall signal output line has three, how should it be connected?
I want to use…
Part Number: AMC1311 Other Parts Discussed in Thread: TMS320F28377D AMC1311的Output common-mode voltage为1.44v ± 50mV ,我想要把它连接到TMS320F28377D的16位ADC上;但是手册中 TMS320F28377D的input common-mode voltage为VREFHI/2 ± 50mV;是不是意味着我要把VREFHI设置为2.88v才可以?但是应该没有这样的基准吧…
Hi Yale:
我回复一下Joseph的问题,麻烦跟进一下,谢谢!
1) As shown in Figure 1 below, the customer's voltage reference circuit, VDDA is 5V, and 3.3V is generated through the voltage regulato
Is VDDA supply and VDDIO supply generated from the same regulator? When these…
Part Number: MSP430FR5994
If I use the data collected by the ADC module that comes with the MSP430FR5994, how should I convert the data format to the array input in the example transform_ex1_fft_fixed_q15 for direct use.
Part Number: CC1310
Hi team, I am using the CC1310 RTOS this code is in a while(1),I found that it's consuming time is about 180ms(approxiately),is the consuming time in this while(1) correct 50kbps rfpacketTX?and then I noticed that the current also…
Part Number: TLV320AIC3204 这是我的寄存器配置
MCLK=24.576MHZ,WCLK=3.072MHZ,BCLK=48KHZ,AIC3204处于主模式,给FPGA提供WCLK和BCLK
# 寄存器 写入数据
0x00,0x00 // Initialize to Page 0
0x01,0x01 // S/W Reset to initialize all registers
0x0b,0x81 // Power up NDAC divider with value …
Part Number: TMS320F28035 我对此并不熟悉,以下内容如有错误之处请您批评指正,如有表达不清的地方请您指正。十分感谢
I am not familiar with this, please criticize and correct if there is any mistake in the following content, and please correct if there is any unclear expression. Thank you very much…
参考下工程师的回复:
Make sure that the PWM and ADC are configured correctly according to the hardware board you used. Check the PWM output and the voltage on the ADC input channel, and then check the related ADC result.
Please take a look at the Universal Project…