Part Number: TPS61094 Other Parts Discussed in Thread: TPS61220 , TPS63802 , TPS61022 , , BQ25173 , BQ25703A 芯片需求:锂电池2.6~4.2V的电压输入,超级电容工作电压最好也可以限制在该范围内,最好是可调版本输出,另外在超级电容后端会接入稳压模块以及负载,稳压3.3模块选用的是TPS61220;后端负载至少需要电流400mA(电压在3.3V情况下);以下是整体的构型:相当于我需要连接锂电池和超级电容的一款单项DCDC芯片…
Part Number: PMP21529 Other Parts Discussed in Thread: LM5170 该方案中电流环和电压环是串联还是并联,原理图中是用Iout1和Iout2作为电流环的输入吗?1k 2.2uf的滤波造成的延迟会对环路造成哪些影响?用2套这个方案的电路进行交错并联共用一个电压环,分别用两个电流环,可以实现均流吗? 和正常工作吗?
您好,看起来是进入了ROM mode
It's possible for the enter "ROM mode" if the checksum stored doesn't match the checksum calculated after a reset. Do the following:
Send command 0x08 to execute FW
Check that the bq40z50-R1 FW is executing
Send command…