Part Number: LMR14030 按我的原理图布线,发现完全不起振,或者说开关频率极度不正常,不知道哪里出的问题,所有器件全换了一个遍,FB信号线与电感是太近了,但也不至于SW信号成这样,完全懵了。电感也从4.7uH,换过6.8uH,也换了22uH,启动电容也换过,RT电阻更是换了好了多个,从10K,12K,20K,22K,47K,68K,
Part Number: TMS320F28035 How do I make the DSP28035 (or any other model) get a three-way Hall signal?
The DSP28035 Ecap input port is only 1, and the single brushless motor Hall signal output line has three, how should it be connected?
I want to use…
Part Number: TPS92690-Q1 Other Parts Discussed in Thread: TPS92690 用TPS92690做的LED光源驱动
【工作条件】
输入:12.8V-16.8V
输出:30V/1A
调光方式:模拟调光
开关频率:200k
【原理图】
【问题波形】
以上~
Part Number: OPA818DRGEVM Other Parts Discussed in Thread: OPA818 您好:
因为opa818的静态功耗十分高,电路板温度已经超过60℃了,每个有25片opa818。
现在想把它的PD引脚用起来,也就是不用运放的时候,将它shuntdown,以减小功耗。
但是,每个电路板25个PD引脚控制起来不太方便,所以我想直接控制±电源的LDO shuntdown引脚,这样走线就少多了
这又有一个问题,参见下图,据说先上负电源,再上正电源…