Part Number: LM3488 Other Parts Discussed in Thread: TIDA-010057 您好,
我在设计一个用LM3488实现的SEPIC直流升压电路, 整体在参考TIDA-010057。我这边希望做一个可以调节的输出电压,但是网上并没有实列。我根据TIDA的说明书进行了一些计算,能否麻烦您帮忙看一下假设及推导过程是否合理。以下照片为说明书的设计截图。
设计我的输出电压可调范围在15V~80V, 输入的控制电压在0V~5V。假设R1跟原设计一样是298kohm…
Part Number: BQ24620 Other Parts Discussed in Thread: BQ24640
1.BQ24620芯片按照资料描述,进入定时故障后VFB电压低于阈值电压0.125V即可退出定时故障,我们测试过程中发现,电池电压很低的情况下进入定时故障即使VFB电压低于阈值电压0.125V也不能退出定时故障,电池电压高的情况下,进度定时故障VFB电压低于阈值电压0.125V即可退出定时故障,资料上没有做出详细说明,定时故障与电池电压有关吗?
2.BQ24620与BQ24640相比不同点有哪些…
Part Number: BQ40Z50 Other Parts Discussed in Thread: BQSTUDIO , 你好,我们目前有从终端客户处客退5pcs产品,表述都为无法正常充放电,产品使用的方案为bq40z50,电池为4串,实际退回定位不良原因一致,都集中在电量计bq40z50部分,针对其中1pc做分析,大致情况如下:
1、电量计部分设计如下,针对不良品确认功能,用Adapter对内充电,PD正常起20V,但LED行为显示过温保护(LED挂在PD IC上),产品无法进shipping…