Part Number: TPS61094 Other Parts Discussed in Thread: TPS61220 , TPS63802 , TPS61022 , , BQ25173 , BQ25703A 芯片需求:锂电池2.6~4.2V的电压输入,超级电容工作电压最好也可以限制在该范围内,最好是可调版本输出,另外在超级电容后端会接入稳压模块以及负载,稳压3.3模块选用的是TPS61220;后端负载至少需要电流400mA(电压在3.3V情况下);以下是整体的构型:相当于我需要连接锂电池和超级电容的一款单项DCDC芯片…
Part Number: BQ25798 Other Parts Discussed in Thread: BQ28Z610 ,
您好!我们使用BQ25798给系统供电并给电池(2芯,BQ28Z610)供电时,当电池温度在充放电保护温度点附近会发生系统重启或关机一次,并且这个重启或关机问题发生随着电池温度保护点设置改变而改变;(我们现在设置为0°,则当电池温度为0°时,会概率出现一次重启或关机,设置为-5°,则问题发生在-5°,如图为电池电量计充放电温度设置);我们现在解决这个问题是需要将BQ25798的TS…
Part Number: BQ27441-G1 Other Parts Discussed in Thread: BQSTUDIO BQstudio版本:1.3.101;系统:win10.我使用BQstudio连接BQ27441后,我用一块电量放光的电池进行循环学习,点击star之后,不是正常的流程,直接就跳到了放电,没有经过等待和充电的过程,目前我无法进行一个完整的循环学习流程。这是什么情况,请教工程师解答,有没有详细具体的教程