This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运算放大器偶次谐波失真问题?

Other Parts Discussed in Thread: OPA820, THS3001, THS3091, LM317, LM337, DEM-OPA-SO-1A

我用OPA820+THS3001+THS3091搭一放大电路,Av = 40dB,当输入信号为10MHz,100mVpp正弦波时,产生较多偶次谐波,失真程度明显比1MHz时严重。
随着频率的升高,失真会越来越严重这个我知道,但是我觉得10MHz的时候失真太大了,从信号源的频谱可以看到,偶次谐波分量很少,但是经过放大之后,偶次谐波越来越多,最后都能看出波形存在失真了,如果我取消级间阻抗匹配(相当于减小运放负载)偶次谐波就没那么多了。我想知道,这偶次谐波失真是怎么出现的呢?


我首先排除了电源的问题,因为电源可以引入偶次谐波,所以我做了一个稳压源,用LM317+LM337做的,发现偶次谐波失真的现象没有改观,可以排除电源的问题。

示波器是泰克MDO3052,信号源是泰克TSG4104A

下图是放大器原理图:

OPA820阻抗匹配之后输出波形及频谱:

THS3001匹配之后输出波形及频谱:

THS3091输出波形及频谱:

信号源波形及频谱:

PCB: