This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BUCK电路构成的恒流源使用运放的选型

Other Parts Discussed in Thread: OP07, OPA209

工程师你好!

我目前设计BUCK电路的恒流源,对分流器上的电流信号通过运放进行放大(构成的差分放大电路放大倍数是39),然后送到ADC中。我的BUCK的开关频率是200K。设计使用的是OP07,但是OP07的增益带宽积只有0.6M,且压摆率为0.3V/uS。是否会导致输入的信号在运放输出失真。因为输入的电流信号是一个频率200K的类似于三角波的信号。此信号用于BUCK环路调整。我这样对增益带宽积的理解是否正确?如果不能使用OP07,请推荐一款TI的运放,最好引脚是兼容OP07的。谢谢!