This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2904B-Q1: LM2904-Q1和LM2904B-Q1以及LM2904BA的区别

Part Number: LM2904B-Q1
Other Parts Discussed in Thread: LM2904, LM2904B, LM2904BA, LM2903B-Q1, LM2903-Q1

Hi

请教下车规级物料LM2904Q1和LM2904B-Q1的区别是什么?LM2904、LM2904B、LM2904BA的区别又是什么?

另外LM2903B-Q1和LM2903Q1的区别是什么?

是否有相关介绍其区别的文档可以提供给我?谢谢!

  • 您好,首先LM2904 工艺比较老,LM2904B是较新的工艺,提高了性能同时价格也比原来低。我们以输入失调电压为例,LM2904B的要比LM2904要低,LM2904的Vos最大为10mV,而LM2904B的最大Vos最大为+-4mV,同样LM2904B和LM2904BA比较的话,LM2904BA的Vos比LM2904B的要好一些。 所以电气参数上我们可以通过电气表格进行对比。

    关于LM2903Q1和LM2903-Q1的区别,首先我没有找到LM2903Q1的型号,它只是在LM2903-Q1的数据手册中提到了两次, 应该是印刷错误,后缀带Q1的指的是汽车级应用产品,并且满足AEC-Q100的汽车标准。