Other Parts Discussed in Thread: PGA280
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应该还没有看仔细吧
Gain is controlled by Register 0. This register can control the gain and address for an external MUX in one byte. Selectable gains (in V/V) are : 128, 64, 32, 16, 8, 4, 2, 1, ½, ¼, and ⅛. The gain is set to 1/8V/V after device reset or power-on.
datasheet Figure44的图是PGA280的输入端内部开关的图,当PGA280上电reset后,默认的是A1,A2关闭,其他开关打开,所以输入信号选择的是INP1和INN1。
如果要使用channel 2,请参考应用手册的Page5的介绍:
For using Channel 2, INP2 and INN2, send this instruction:
L 66 18 H ; This command activates the BUF stage and connects INP2 and INN2 to the amplifier.