Dear all:
DAC output 0-5V is amplified to 28V through OPA187. May I ask if the R15, R17, and R20 parameters are configured correctly? Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您是需要将最大输入信号5V放大至28V吗?这是个同向比例放大电路,放大增益是6倍(10K/2K+1=6),输入0~5V,当输入信号到达5V时,放大6倍输出是30V,而不是28V,因此这个参数并不能满足您的要求。
5V放大至28V,增益是28/5=5.6倍,可以使用TI的Analog Engineers Calculator工具设计电路参数:
Analog Engineers Calculator下载链接:https://www.ti.com.cn/tool/cn/ANALOG-ENGINEER-CALC?keyMatch=ANALOG%20ENGINEERS%20CALCULATOR
同时注意运放的供电电压满足输出要求。
运放供电电压使用30V没有问题,如果您是通过DAC80501输出电压将运放输出电压控制在28V的话,那么在增益为6倍的情况下,DAC输出最大不能到5V,大概为4.66V。
建议短接R15电阻,在运放同向输入端串联电阻一般是为了抵消运放的输入失调电流,但是运放 OPA187 在生产时已经做了校准,如下截图所示其输入失调电流是± 双向的,因此串联电阻并不能100%保证可以相互抵消,还可能加倍产生的失调电压。另外也建议您看下下面文章: