您好,就是我们需要测量大约200V共模电压下微安级别的电流,请问INA149可以支持嘛?如果支持的话,请问采样电阻大概可以取多大?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
支持的,INA149最大可支持的共模电压到 ±275 V,但是需注意供电电压的选择,因为供电电压限制可以输入的最大共模电压,具体见如下截图描述:
INA149的差分输入和输出范围在电源轨的1.5V以内,即(V- +1.5V) 至(V+ -1.5V),因此选择采样电阻时,需考虑检测的电流范围,使得差分电压满足INA149的规格范围;另一方面,虽然采用电阻越大,测量精度越高,但也需考虑系统允许的采样电阻的最大电压降,电阻越大产生的功耗越大。
TIPD135 这个参考设计中有对采样电阻选择的考虑的描述,具体见下面用户指南:
10-uA to 100-mA 0.05%-Error High-Side Current Sensing Design Guide