This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA214: if GND pin can use negative voltage

Part Number: INA214

In my design, I want to sense about 10-600mA current use 0.045ohm current-sensing resistor. I am concerned that the output may be nonlinear when detecting small currents, so I want to give negative voltage like -5V to the GND pin and short REF pin to system GND. If INA214 can work normally when using negative voltage with GND pin.

  • 您好,

    您是担心在小幅值输出时,不在 INA214输出范围是吗?

    您可以在INA214 REF管脚接一个电压,让INA214 输出以此参考电压输出。如果您测量的电流是双向的,一般REF管脚推荐接供电电压的中间值,即若5V供电,REF接2.5V,这样输出在2.5V基准上上下摆动。

  • 我的设计中只会涉及单向电流。我可以在REF pin上供一个特定电压,比如0.2V,但是这个0.2V的电压精度我比较担心。我想,如果能在GND pin上添加上负电压并在REF pin接系统地,就能保证低电压输出时的线性度跟精度,所以我想确认下GND pin上是否允许接负电压并在REF pin上接系统GND。

  • INA214的GND可以接负电压,从放大器结构上讲,它在工作时无法分清自己是被双电源供电,还是单电源供电。任何运放的两个电源端只要满足有足够的压差,运放就可以工作。但是这会影响输入和输出范围。

    INA214的GND接负电压,那么输入端电路的参考点将变成这个负压。INA214的REF pin接地,那么INA214的输出将以地为参考点输出。

  • 了解,感谢。

    1.假如INA214的V+我接入+5V,GND pin接-5V,REF pin接 system GND,那输出的范围是否为-5V+0.05V~+5V-0.2V?

    2.GND pin接-5V的话,按我的理解,不会导致器件性能下降对吧?

  • 1、理解是这样理解的,但输出范围具体取决于输出负载,0.05V 和-0.2V是在10kΩ to GND条件下给出的。

    2、我理解不会导致器件性能下降,虽然datasheet 给出的是在单电源: VS = 5 V下的电气特性参数。