采用PGA206标贴封装的放大器,但是当在VIN+引脚输入+5V直流电压,在VIN-输入GND时,为什么输出引脚与地间的电压只有3.2左右呢?引脚连接如下:1、2、3悬空4接地,5接+5V直流电压,6、7悬空,8接-15V,9悬空,10接地,11和12相连作为输出引脚,13接+15V,14接地,15、16为可控引脚。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用PGA206标贴封装的放大器,但是当在VIN+引脚输入+5V直流电压,在VIN-输入GND时,为什么输出引脚与地间的电压只有3.2左右呢?引脚连接如下:1、2、3悬空4接地,5接+5V直流电压,6、7悬空,8接-15V,9悬空,10接地,11和12相连作为输出引脚,13接+15V,14接地,15、16为可控引脚。
你好,
请问15,16脚是怎么接的?如果15,16脚也是接地,输出应该是5V。
你可以测一下9脚和1脚的输出吗?
引脚9输出是3.3V左右,没有问题吗?传电路图有点困难,因为是保密单位。但是从+vin和-vin之间测量的电压是5V没有问题,输出引脚接到了AD芯片的输入引脚上了,还有就是15,16脚在FPGA给00之前是用排阻拉高的。就这,别的什么也没有连着这个增益放大器了。会不会是这个片子本身坏掉了呢?