用于制作简易基于fpgs的dds 输出频率为1M 输出后需接椭圆滤波器进行滤波 设计时采用两片opa690做阻抗匹配
前级为同相输入 射极跟随 后级为补偿增益 增益为2的反相放大
但现在想要提高输出幅度 峰峰值有10v 可以采用什么型号的运放新型替代 opa系列的大供电电压的型号好像很少
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
可以看看 THS3092 THS3001 THS3095
你好。
因为你是做波形发生,虽然输出频率是1Mhz,但是如果是方波发生的话,由于谐波分量的缘故,要求至少10倍以上的带宽。
一种比较通用的办法是:前级用OPA695/THS4271做输出信号buffer,后级用THS3091/5做大幅度/高带宽/高电压驱动。