尊敬的TI工作人员:
我想请教一个OPA593引脚连接的问题,我不使用OPA593的过电流和超温标志、热保护、输出禁用等功能,只是把OPA593当做一个普通的运放来使用,也不进行电流限制,直接以最大输出电流250ma输出;
我需要使用两个OPA593,其中一个供电为+80V、-5V,另一个供电为-80V、+5V,请问OPA593的EP、E\D、E\DCOM、LIMIT、ThermalFlag、CurrentFlag引脚该怎么连接?
期待您的回复,感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的TI工作人员:
我想请教一个OPA593引脚连接的问题,我不使用OPA593的过电流和超温标志、热保护、输出禁用等功能,只是把OPA593当做一个普通的运放来使用,也不进行电流限制,直接以最大输出电流250ma输出;
我需要使用两个OPA593,其中一个供电为+80V、-5V,另一个供电为-80V、+5V,请问OPA593的EP、E\D、E\DCOM、LIMIT、ThermalFlag、CurrentFlag引脚该怎么连接?
期待您的回复,感谢!
Overcurrent Flag和Overtemperature Flag不用的话悬空。
ILIMIT可按照250mA,接2.29kΩ到V–。
E\D和E\DCOM可按照数据表 图 7-3. E/D and E/D Com Pin Connection左边图接。
应该是可以的。数据表没有明确的说明,建议您仿真或实际实验试下。