现在有一常见的AV信号,包括一个CVBS,一个左声道,一个右声道。3部分。做AV 一分二操作。初步预想是用4053,刚好3路1分2开关,一个信号用一路。不需要同时具有两个输出,同一时间有一个信号输出就行,实际则是1进1出的概念。但是这里有以下几个疑问,还望大神指点
1:是用74HC4053还是用CD4053呢?因为既有视频也有音频,不知道如何兼容才好,系统里面是12V输入,里面有5V,3.3V,1.2V等电源。
2:网上很多人说4053出来的要么视频信号不好,要么音频有串声等。但是又很多电视好像都在用这个。很犹豫,是否要用这个产品,如果要用,该如何去设计此电路避免出现问题,分配过后后端是否需要加运放啥的。负电压是否一定要用了才好?因为如果加入负电压,又让设计更复杂了。也增加成本。
3:或者,是否有更好的芯片方案推荐呢。