IAR Patch Install
----------------------
Note: Below step is required only for IAR 7.2 or lower only(must not be done for IAR 7.3 or higher)
1. For FTDI based CC32xx device, copy "armLMIFTDI.dll" to "C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.0_2\arm\bin" 

IAR  : Debugging Using FTDI
---------------------------

1. Open the project
2. Goto Project->Options->Debugger->Setup->Driver and select 'TI Stellaris' from the drop down.
3. Press Ok