TI 诚邀您参与论坛问卷调查,帮助我们改善技术支持体验。几分钟便可完成,将随机抽取30名用户送出快充数据线,点击参与

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825M: Double SPK scheme.When no audio data is input and Automatic mute state, there is a idle noise in the speaker.There is also noise in playing music.

Part Number: TAS5825M

Description of test phenomena:

1、SDIN pin has no signal input.

2、LRCLK and SCLK signal input is normal.VR_DIG voltage 1.496V,GVDD voltage 5.10V,AVDD voltage 5.18V.The ripple was less than 12mV.

3、The impedance of SPK is 8 ohm.PVDD voltage 24V.

4、Adjusting gain has no effect on idle noise.

  • 您好,

    idle状态下,您测得的噪声幅值是多少?您选择的是什么调制方式?PCB您是4层吗

    在播放时有噪声,您可以用示波器实测一下输出波形吗

  • Amy Luo,您好:

          我们这边每块板子复现现在还不太一样,都是人耳可听到的噪声,小的时候大约5dB,大的时候20-30dB;,PCB为四层板,第二层第三层都是地层;Hybird 和BD模式都有尝试,下面是同事手中板子的现象:

    1. yh的板子: Hybrid模式,播放非静音或静音数据时,都会高概率出现持续的噪声,噪声有大有小。BD模式,暂未听到噪声,也没有电感发热现象。

    2. xt的板子: Hybrid模式,播放非静音或静音数据时,都会低概率出现持续的噪声,噪声较小。BD模式,有电感发热现象,暂未听到噪声。

    3. fm的板子(只测试了一次): Hybrid模式,启动后播放非静音或静音数据时,听到持续的较大噪声。BD模式,电感有发热现象,启动后播放非静音或静音数据时,暂未听到噪声。

    4. yx的板子:Hybrid模式,启机后约播放静音数据50s出现滋滋声持续2s,之后就没有听到噪声。BD模式现象一样,电感没有发热。

    以下是有噪声时,测得的喇叭单端波形。

  • 更新BD调制模式持续发出噪声的一块板子的OUT_A+和SPKER单端波形,OUT四个引脚与喇叭引脚测到的波形一样。频率392Hz,均方根10V。

  • register0x53h-D[6-5])和register0x02h-D[6-4]您配置的是什么?

    您输入的LRCLK SCLK信号频率多少,用示波器实测波形怎样?

  • 您有TAS5825MEVM板吗?拆下电感做下交叉实验

  • 原因找到了,谢谢您。

    具体现象如下:

    1、进程启动时候,spk±波形,出现过冲,差分后峰峰值>2.7V.

    2、随后直流分量和交流幅度值不断变小,此时spk±同相位。

    3、第59s相位突然发生变化。产生噪声。对应out_A±波形发生时序偏移,且高电平占空比变小。

  • Hybird Mode产生噪声原因为:

    Hybird Mode未按照(Base / Pro Hybrid (2.0 48k))生成.h文件。上述现象为按照第一列96K生成参数所致。

  • 很高兴您的问题得到解决,非常感谢您的反馈

  • 您好,Amy Luo:

  • 您好:Amy Luo ,我们播放1khz音频信号,输出波形单端,会叠加开关频率384Hz,调制模式为混合调制,请问这一般是什么原因导致呢?谢谢。

  • 开关频率您配置的是384KHZ是吗?那Loop Bandwidth配置的是多少,即register 83 -Register address 0x53h-D[6-5]配置的是什么值?在Hybrid调整模式下是需要Fsw (Switching Frequency) ≥ 4.2 × Loop Bandwidth