Other Parts Discussed in Thread: TAS5825M, , TAS5805M
DRC=ON, the power from -12dB to 0dB is different, for example, -7dB=7.4W,-2dB=8.8W,0dB=8.5W. How to adjust the -7dB output to be 8.4W as 0dB output
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
TAS5707 is NOT Recommend For New Design. It would be obsolete. So I recommend you consider other similar product to replace, for example, TAS5825M and TAS5805M.
您好,因为TAS5707现在为NRND状态,所以之前有一篇针对TAS571x和TAS570x系列的关于如何控制DRC的应用手册也在官网找不到了。
您是考虑更换TAS5805还是针对5707的DRC控制需要了解?如果需要这篇DRC控制的应用手册,我需要去确认以下。
好的,关于DRC控制的应用手册我这边再去确认一下。
您好,参考这篇TAS57xx系列DRC的应用手册:
您现在测得-7dB比-12dB功率要低吗?
看这个曲线是成正比例呢。
您好,这个是推荐的初始配置,当然客户可以根据自己的应用需求进行微调。
您好,Energy(ms)控制平均窗口时间用于确定平均信号能量,因此,输入信号与设定的DRC曲线比较,它是控制给定频带的DR时间常数,避免由DRC attack和输入信号频率造成的音调跳动。 具体可参考这篇应用手册的16.7部分的介绍
https://www.ti.com/lit/an/slaa786a/slaa786a.pdf
您好,为了更好的跟进您的问题,建议您重新发个帖子咨询。